Want to save up to 70% power consumption?
– Then choose the right solar pump!
Dimensioning of the solar system to the required thermal output affects what
flow is needed as well as the pressure loss in the system. A typical forced circulation
solar system runs with a flow between 0.1 – 0.5 m3/h with a pressure
loss between 200 to 400 mbar.
This greatly influences which type of circulator is optimal to integrate from a
performance and energy consumption perspective.
Normal standard circulators – which are widely used in solar thermal systems –
are designed for optimal performance at a much higher flow (usually between
2-2.5 m3/h). The result is substantially higher energy consumption than necessary.
To solve this issue, we have developed the world’s first optimised solar pump,
saving you up to 70% power compared to normal solar pumps!
Here you can see how we have reduced the power consumption of Grundfos
solar pumps over the years:
”Grundfos Solar”
Circulators for solar thermal systems
Download (PDF 313 KB)