Low energy and high performance The unique energy saving features of the MAGNA pumps ensure maximum efficiency combined with a minimal use of energy – for both heating and air conditioning systems.
Part of the secret is our patented AUTOADAPT function which is integrated in all 28 MAGNA models and which ensures a performance curve that is always adapted to match the needs of your particular system.
As a result, all MAGNA pumps are rated ‘A’ on the European energy labeling scale. A result we are very proud of at Grundfos because it means both lower costs for our consumers as well as better conditions for the environment.
The bottom line The energy efficiency of the MAGNA pumps makes them the obvious choice for the cost-conscious consumer.
Below, you can see how much you can save every year by simply trading in your old pump for a new MAGNA pump.
All you have to do is type in the relevant data in one of the two tables. Use the first table if your current pumps are from before 1997. Use the second table if your current pumps are from after 1997.