Designed for
installation below floor level, the Liftaway B provides
a simple solution for existing buildings where wastewater
has to be pumped to the sewer system.
The Liftaway B is ideal for pumping wastewater from washbasins,
washing machines*, sanitary rooms, showers, floor drains,
etc. It can also be used as a drainage pit for pumping drainage
and surface water. The Liftaway B can be used in combination
with a stainless steel Grundfos KP or AP 12 pump with float
switch for automatic start/stop. (The pump must be bought
separately.)
* Max 70OC for two minutes.

|