homecontactgrundfos.comlegal issues Grundfos SP
 
   
 


Water utility companies are constantly on the lookout for ways to optimise water catchment and to reduce well field inspections.

When I/S Ikast Waterworks decided to build the new Bogild Waterworks and establish a new well field, the company therefore installed the most modern surveillance and control equipment available.

The situation
To ensure maximum profitability, the Danish water utility I/S Ikast Waterworks needed to both optimise its water catchment processes, and keep the costs of well field inspections down.

Setting up the new Bogild Waterworks and a new well field at the same time presented the company with an important opportunity to optimise both these operations.

The Grundfos solution
The Ikast Waterworks requirements focused on maximum reliability with a minimum of inspections. The company also wanted more detailed documentation of the water catchment.

The main contractors, HOH Water Technology A/S, decided on installing Grundfos SP pumps along with Grundfos pump control units fitted with the sensor, SM 100 extension modules. These high-efficiency units are installed at all five well fields currently in use. They are linked directly to the waterwork’s PLC via Grundfos GENIbus communications protocol, for fault-free remote monitoring. In addition, all operating data can be collected using a Grundfos R100 remote control unit.

The outcome

The combination of Grundfos SP pumps, Grundfos pump control units and the technology to link them together gives Ikast Waterworks optimal control over its new borings, with no need for costly on-site inspections.

The company is now able to monitor the state of the entire system as well as each individual well, and also able to supervise the efficiency of all the elements in pumping operations. The engineers can easily identify any irregularities and significant trends in the data, which means that they have the best possible information at hand for optimising all aspects of operations at the new Bogild Waterworks.


Grundfos products used
  • SP pumps
  • MS motors
  • SM 100
  • R100
  > Download a more extensive version of this case history as a PDF file.

CONSTANT OPERATING OPTIMISATION OF RAW WATER CATCHMENT