homecontactgrundfos.comlegal issues Grundfos SP
 
   
 


Carbon-filter system in waterwork, Rheinau der MVV Energie AG

The situation
MVV Energie AG is an international distributor of energy and services - a modern multi-utility group.

With a total turnover of 1.2 billion Euro and some 3,500 employees, the group is one of the biggest regional distributors of energy in Germany, and ranks among the most innovative enterprises in the market.

In the Kafertal and Rheinau waterworks, MVV operates 85 water extraction wells. The high iron content in the groundwater combines with oxygen to produce massive ochre deposits on the inside of the cast iron pumps.

"For pumps in the shallow boreholes, the ochre builds up quickly and the pump only performs [at] 50%," says Werner Faschingbauer of MVV.

The Grundfos solution
Now, more than 30% of the company's wells are equipped with Grundfos high-grade steel SP pumps (in new installations this share is nearly 50%.).

Herr Faschingbauer also uses the new Grundfos infrared control unit. He can change factory settings and monitor the installation of a pump by remotely calling up actual operating data (e.g. current consumption, supply voltage, operating hours).

The outcome
  • Quality materials. "In our opinion the deposits on the smooth high-grade steel surfaces of an SP pump stick less firmly than on the rather coarse cast iron. It's also easier for us to remove the ochre scale."

  • User-friendly. "You don't need to have any specialist knowledge. All units are of the same design - once you have dismantled and reassembled one of these pumps, you know what's what."

  • High efficiency. "In this field Grundfos now has a leading edge."

  • Reduced Cost of Ownership. "Now we use the diagnosing unit to test the units that fail to run."
The SP pumps and CU3 are integral parts of a cost-effective and reliable water supply.

> Download a more extensive version of this case history as a PDF file.

Grundfos products used
  • SP pumps

LARGE SP - SIMPLE HANDLING, HIGH EFFICIENCY