Why focus on Cost of Ownership?
The simple answer is that you can't afford not to. Cost of Ownership is a way
of thinking.
It starts right from the moment you decide you need to pump water from one point
to another. And it doesn't stop until the pump has served its optimal lifetime.
For further details download the Cost of Ownership brochure |
|
There's more to it than meets the
eye
Cost of Ownership is about thinking ahead and knowing what lies beneath the surface
- maintenance costs, energy costs and the benefit of having a business relationship
with Grundfos.
For more details download the
Cost of Ownership Powerpoint
presentation
|
|
Typical lifetime cost-split for
a groundwater installation.
An important part of Cost of Ownership (CoO) is Life Cycle Cost (LCC).
Measurements have shown that seen over the pumping system's entire lifetime,
initial cost is only 5%, maintenance cost is 10% while energy cost counts for
85%. |