home contact grundfos.com disclaimer  
Imagine Benefits Product features Performance curves FAQ Cases & references Download
Grundfos SQ/SQE
 
  CONSTANT WATER PRESSURE
 
 
  The benefits of the SQE are numerous, but none can outweigh constant water pressure. This is the benefit that people consider a luxury when they first have the Grundfos SQE/CU301 package installed in their home. However soon they learn to take it for granted. Which is the way it should be of course. Life is full of things to worry about, and the list doesn't need to be added to. Get what you expect when you turn on a tap. It's as simple as that.
 
> CONSTANT WATER PRESSURE
> ADJUSTABLE WATER PRESSURE
> FULL PERFORMANCE INDICATION, BURNOUT PROTECTION AND FAULT DETECTION
> EASY TO USE