Note: Figures in () are KP 350 values
Installation
Pumps without level switch or with float switch can be
used in vertical position with the discharge port uppermost or in horizontal or tilted position with the discharge port as the highest point of the pump.

|
|
Level switches
A level switch, which gives impulses to start/stop
between two levels of liquid, is connected to pumps
intended for automatic operation. This type of installation
requires a non-return valve in the discharge pipe or
pump. The pumps are available with two different types
of level switches.
Minimum liquid level
• manual operation: 14 mm
• automatic operation: See below.
Pumps with float switch
A clamp on the handle of the pump holds the cable of
the level switch. The difference in level between start
and stop can be adjusted by changing the free cable
length between the handle of the pump and the level
switch.
Dimensions for Unilift KP 350 are marked with an "*".
Pumps with vertical level switch
For pumps with vertical level switch, the difference in
level between start and stop is not adjustable.
Dimensions for Unilift KP 350 are marked with an "*".
|